PG2 elements for Touchscreen use
Does anyone have experience with touchscreen elements configuration on PG2. Are there any usable library elements for touchscreen use, like a slider etc?
Answers
You do not distinguish between PG2 elements for touchscreens and ordinary screens. All PG2 elements are usable for touchscreens and all the elements you need are available.
The biggest challenge is to make a display and workplace design that is suitable for touchscreens.
The biggest challenge is to make a display and workplace design that is suitable for touchscreens.
Touchscreens are not directly supported at this stage (ie not fully tested). If you do wish to use 800xA with touchscreens there are a few thigs to keep in mind: our fingers are larger than a mouse pointer. This means larger screen items and more space around them, so selection can be precise. In the past I would use my fingernail as the 'footprint' of the object size on the screen. The 800xA Workplace is not ideally suited to a touchscreen as the icon sizes are too small and not adjustable.
Just for information.
I found a solution in the DragHanlder and RotateHandler. With this you can move objects or bars on the screen.
Add new comment