Using CI867 with PM865 HI Controller
Greetings,
We're using both SIL and Non-SIL applications with PM865 HI Controller.
For our facilitiy, we have to use an operator panel,thats why I'm trying to add CI867 Modbus TCP card.
But during download session, we faced an error message. This mesaage says: "The communication protocol in connected library for CI867 at position 8 is invalid" (Please see attached picture, for details.)
How can we fix this error?
Thanks for you help.
Voted best answer
In 800xA System there are two different CI867 hardware Lib is available.
CI867 1.1.81 for AC800M HI Controller (Safety)
CI867 20.0.38 for AC800M Controller (Process Automation)
Add new comment