MFP12, Getting started
I use MFP12 (with NTMP01) only inserted into MMU21, and when i turn power on all LEDs on MFP12 are red. I trying to initialise module by the SW4, but without good results. Am i must to insert any additional modules into MMU or it's enought to make connection between Composer and MFP12?
Voted best answer
I guess you need to understand the Infi90 system a little bit more. The MFP should run on it's own (LED 7 & 8 lit) without any other supported cards or modules. However the MMU power wiring and earthing should be setup correctly. Unless you have a faulty MFP module. For the MMU get the wiring for the card cage and ensure you have +5VDC, +/- 15VDC and usually 24VDC (for the TMP). The TMP is not needed unless you need RS232 interfaces or other older HW...
Add new comment