Freelance 2016 Diag port
Today I test the new FREELANCE VERSION 2016.
I have a surprise when I connect my serial cable to the Diagnostic port in the AC900 controller to change the IP.
I receive estrange characters and I can’t read anything.
I check the cable, HyperTerminal configuration (9600 8N 1 hardware) but It doesnt work, finally I downgrade the Firmware to version 2013, in this version the port it works like until now.
There are new parameters, speed, parity, terminal emulation … for the diag port in this new 2016 release?
Answers
Greetings,
Please find below link, similar question has been asked before:
http://www402.abbext.com/ip-configura...
Hope it helps you.
Hello!
From Freelance2016 on the diagnostic interface runs with 19200 Baud.
See ReleaseNotes or Mounting&Installation Manual of that version.
Add new comment