Ethernet/IP Communications between AB ControlLogix and ABB AC 800 Controller
Hello,
We will be attempting to establish Ethernet/IP communications between a Rockwell ControlLogix Processor and an ABB AC 800 series controller. The communications will be initiated in the ControlLogix environment. Is there a standard method to established communications, over Ethernet/IP, such as “Assembly/Instance” Connections (done with ABB Drives) or MSG Instruction type etc?
Answers
Hello,
If you have access to partner portal then check webinar recording on 'Ethernet IP Integration in AC 800M' on 6th Agust. if no access, request for partner portal access via your local ABB representative @ http://www.abb.com/MyABB/Partners/Default.aspx?country=US&c=77dbff815717334
ac1257df70000d82f&db=db0003db003390&ap=1 OR you can find link for Partner Exclusive webinars at righthand side column of this forum
Hope that helps...
Add new comment