AC800M Load
Does any tool exists to calculate the load of AC800M?
Say 1) Load of Profibus modules/tags on AC800M
2) Load of Modbus TCP on Ac800M
3) Load of IEC61850 on AC800M?
Please guide
Answers
Hello,
There is a system Library for this,and its an excellent feature too.
I can not exatly recall the exact name of it.
But is present in one of the System Libraries of 800M controller builder.
What I can recall the name is similar to :
"SystemEventtime.." or
"SystemDateTime.."
you have to just connect that Library. and attach it into the main application.
Then it has two feature either you can See it as FACPLATE by right clicking it, Or you can call it as a Function Blonk in your program.
It has availability for System Load, Scan time, No of Ethernet Packets live transfer , system Time ,etc features.
Hope it helps.
(I can share the exact name soon)
Add new comment