Is it possible to have different user rights for controlbuilder 800xA
One of our customers if having an engineeering client with control builder, always on-line
They would like to have user rights on control builder.
1) view rights -> view code
2) minor right -> force sequencer to next step, change value of variable. (If system is in edit only online rights, no download)
3) "adminstrator"rights -> full rights in control builder
Answers
Hello,
Generally for CBM activities are password oriented rather than setting view/admin/system eng, are xA roles to use the 800xA for operation.
If you want the customer to open the CBM then it needs application and system engineer role then set the password for each application(Caution: once password has been forgotten you can't reset back again).
then for all users CBM applications will be view only, then for edition it needs password prompt.
Add new comment