S800 IO profibus DeltaV
has anyone ever connected S800 IO up to a deltaV Controller via profibus?
modules here are AI810, AO810, DI810, DO810 and the same in the 890 series.
there is a potential project here that would like to do the same. I would like to get feedback from you.
Voted best answer
Profibus in an independant protocol....
I have already done a demo regarding a Siemens Controller with S800 I/O and a ABB PM controller with Siemens I/O.
All the communication were in profibus and there is no particular restrictions regarding the implementation.
See the attach file "architecture.pdf".
I have already done a demo regarding a Siemens Controller with S800 I/O and a ABB PM controller with Siemens I/O.
All the communication were in profibus and there is no particular restrictions regarding the implementation.
See the attach file "architecture.pdf".
Answers
As FAVRE stated - Profibus is independent protocol. I didn't connect S800 with DeltaV, but Siemens ET200M - yes.
Hi,
Found on google 8 years back someone had similar question...
@ http://control.com/thread/1026248744#1026248744
Add new comment