Sntp setup error
Hi All ,
every time i try to make setup Sntp for AC500 using PM583-ETH it fail , and plc can't put PLC in run mode and i have error code on PLC screen { E4 034 ,d1 10,d2 255, d3 4 , d4 5 }
kindly helping me in this case.
Thanks all,
BR,
every time i try to make setup Sntp for AC500 using PM583-ETH it fail , and plc can't put PLC in run mode and i have error code on PLC screen { E4 034 ,d1 10,d2 255, d3 4 , d4 5 }
kindly helping me in this case.
Thanks all,
BR,
Voted best answer
Greetings,
In your situtation error codes are related with SNTP.Error messages mean like that:
* SNTP: Error finding connection to server, tried 5 times to get connection.
* SNTP: Error time, time difference makes time jump necessary , but too long
* SNTP: Could not sync time before configured timeout.
In my opinion you are making some mistakes on configuration parts. Please see below link for AC500 SNTP Manual:
http://www.infoplc.net/files/descarga...
Hope it helps you.
Add new comment