anyone can explain the meaning of the alarms/events showing in PC Motor Bidirectional Function block .file attache
anyone can explain the meaning of the alarms/events showing in PC Motor Bidirectional Function block .file attached
||SL_FB_{1}\Stop||SL_SC ..........etc
Answers
NLS resources are missing. Ask the vendor of the object type library for assistance.
by Harsha.D
It looks like NLS is not configured properly
Add new comment