IBA PADA connection
How do i connect data aqusation system IBA Pada to 800M other then OPC server.
Can i connect directly via ethernet.
Answers
Communication of IbaPDA can be possible in different ways such as :
(i) TCP/IP Generic
(ii) TCP/IP Modbus client
(iii) Ethernet IP
(iv) DPM-S : This works like a Profibus slave and sends the data through fiber optic to Iba-PDA
(v) The internal card L2B (computer PCI card) that also works as Profibus Slave.
-
Reference purpose you can have look on the follwoing link under heads of Interfaces in iBA PDA :
http://www.iba-ag.com/en/products/software/ibapda/
For reference purpose, you can have look on the attached file.
Add new comment