Error when download AC800M with CI873 and FlexIO modules
We are trying to communicate FlexI/O modules through EthernetIP using CI873. We have 1794-AENT (Ethernet adapter for IO Modules) and AI, AO, DI, DO modules.
We receive errors like following when we try to download (screenshot attached):
"Error 9080: CPLC302:HW Unable to get configuration Parameter Number = 254 for the device at 1.2.6"
This happens just when we add AI (1794-IF8IH-A) or AO (1794-OF8IH-A) modules. If we delete those modules downloading perform without any problem!
Any ideas or hint in how to resolve this will be helpfull.
Regards,
Ignacio
Answers
you should check the file that you used for integrate the modules,
in the past we work with this kind of files, it have some options that could be modified, you can edit this files using notepad.
in the past we work with this kind of files, it have some options that could be modified, you can edit this files using notepad.
Add new comment