E-Mail Configuration Error
Hi Everyone,
I configure the all e-mail seting and When I try to sent mail,TestmailObj give me en error code.Code is attached.How can I solve this problem?
Answers
Hello ,
For Email configuration in 800xA it is require to connfigure Email device aspect first which is available under Aspect System Structure >> Messenger >> Email Device , Aspect Type >> Email Device , Aspect category >> Email device aspect.
For the screen shot you have attached I observed that you have not configured SMTP Relay server .
Hi Fiends,
I have the same error with the email configuration. I have a 800xA system with Workgroup configuration. The SMTP Relay Server has configured to accept the connections from 800xA Aspect Server by Default Gateway address and the 800xA has configures as manual say (Email Device, IP address, Port, email destination, Messenger Email on Service structure, User)
I have a few questions:
1. My User is a part of workgroup but is not the same users in Domain Controller in Network Plant. I need configure the same users and groups?
2. In the Aspect Server I need install the SMTP server feature? The SMTP Relay Server is in the Plant Network.
I need configure anymore for this functionality?
I have the same error with the email configuration. I have a 800xA system with Workgroup configuration. The SMTP Relay Server has configured to accept the connections from 800xA Aspect Server by Default Gateway address and the 800xA has configures as manual say (Email Device, IP address, Port, email destination, Messenger Email on Service structure, User)
I have a few questions:
1. My User is a part of workgroup but is not the same users in Domain Controller in Network Plant. I need configure the same users and groups?
2. In the Aspect Server I need install the SMTP server feature? The SMTP Relay Server is in the Plant Network.
I need configure anymore for this functionality?

Add new comment