CM572-DP Programming
Dear all,
I am new to ABB.I have exp in AB PLC system. I have to control 10 nos of Bernard control intellibus MOV valve through profibus communication with PM583-ETH CPU. I have added *gsd files and configured IOs also. Pls let me know. is required Sycon.net software for configure Profibus master and slave, download configuration to profibus master CM572-DP. I am using Control plus builder 2.3.0 version but i cannot see sycon.net software under Resource-->Tools--->Notepad.
Pls advise me.
Thanks alot.....
Answers
No need for Sycon.net software...
You can add profibus master and slave in Control Builder software itself.
Please find attached snap shot for your reference.
Hello!
You do not need Sycon.net. It is for programming CPU's with firmware v1.xx.
The download is done when you download to your CPU. A major leap is usage. Remember create boot project.
You just add device in the configurator using right click add on your master CP572.
On the device you right click and add how much memory you want to use.
BR
Gustav Andersen
by ranjithiru Rank: 5934 on 12/14/2015 1:34:38 AM | Like (0) | Report
Hi, 24VDC supply is need for CM572_DP. pls confirm.
Add new comment