pidCC in control builder
HI everybody
i have a PID with pidcc control module
i need use "Enable out ramp man"
when is true this value in interaction window if i change the output, value change by out rate increment but if i use faceplate or change variable in control builder the value is not correct
an example:
in manual mode:
using interaction window
initial value out man = 25 change to = 20 result 25 reduce to 20 by rate value
value = 20 change to = 40 result 20 increase up to 40 depending by rate value
error, using write value in control module on line in control builder
initial value out man = 25 change to = 20 result fall intenpestive to 20 and increase value up to 25
initial value out man =25 change to 40 resutl rise inmediatly to 40 and decrease value up to 25
im using the same variable (OutManValue)
could you help me pleasse
thanks
Add new comment