HP T620 thin client OS upgrade
Hi,
We are using HP Thin Client T620 with 32 bit OS Windows 7 embedded. Now we want to go to 64 bit.
Is it possible. Has any one done this before.
HP websites do not provide a clear answer.
Answers
What do you think you wil gain from that on a thin client? Normally you just use rdp to connect to a server or workstation and there is no need for 64bit.
After a long chase and ping-pong between Microsoft and HP, conclusion is "You can not upgrade 32 bit OS to 64 bit OS on a thin client. You need to order seperate hardware."
yes you can you have to upgrade the ram to 8gb and the ssd to 32gb or more
Source: HP
Add new comment