modbus s7-1200 - to ACS580 inverter
Hello
im have plc s7-1200 1414 and motor inverter ACS580. Pleas can you show me how i sent command to write or read from inverter. Im need only simply example for start stop and change speed. Pleas help me.
Answers
Greetings,
Here is an ABB Control System forum, so you can not find any Siemens based program example, etc.
You can find more details about S7-1200 at Siemens forum, please see below links for more details:
https://support.industry.siemens.com/cs/document/63696870/sinamics-v%3A-speed-c
ontrol-of-a-v20-with-s7-1200-(tia-portal)-via-uss%C2%AE-protocol-modbus-rtu-wit
h-hmi?dti=0&lc=en-WW
https://support.industry.siemens.com/...
You can find example codes at there, if you still have some problems about ACS drive modebus parameters etc. We are here to help you.
Add new comment