Bulk Data Manager (BDM) Insert sub-objects from Control Structure into Functional Structure
Hi,
We have some PLC Connect objects that exist in Control Structure and Functional Structure.
In the Control Structure they are like this:
Parent object
--Child object1
--Child object2
...
--Child object 100
In the functional Structure only the Parent object is placed.
What I want to do is to place the Child Objects in the control structure under the correct Parent Object in Functional Structure.
I can do this by pressing "Insert" on the parent in FS, and browsing to the correct child in CS. But there are a lot of tags, so I'm interested in doing this with BDM.
When I try I get "You may not place signal types here". I did one manually, and tried to start BDM with the FS aspect on that one, editing the name to another child I wanted to place. If I included the CS aspect, the system created a new child object with the same name in the CS as well.
Unsure if this is PLC Connect specific or not.
System is 800xA 5.0 SP2
I would much appreciate some help or pointers on this.
BR, Torbjørn
Answers
Hi torb,
I have the same issue I mean I need to add a lot of signals from control to functional structure.
Have you find solution how to do it using BDM?
Add new comment