keep the selection mousepointer, if the mouse is over a disabled inputfield on a graphic element
When I cross the mouse on a graphic element (with the property enableInput=True) in a PG2 display on runtime, the mouspointer changes to selection pointer for full area of the graphic element. But if the graphic element conatin a disabled inputfield, the mouespointer stay a normally mouspointer for the inputfiled area. It's possible to have a selection mousepointer for the full graphic element area, if the graphic element contains a disabled inputfield?
Answers
Hello,
change the mouse pointer in the contol panel for the user and check again.
Add new comment