mineral library PCC viewer
Hello
In our project system800xA we are using mineral library ver5.1 .The system is working perfect but when we open PCC viewer window in consumer faceplate we can't see list of all iterlock signals that are interlocked with consumer via PCC bus.Also I caoud'nt find PCC Uploader aspect to upload PCC tags to update PCC viewer lists.Please help me to fix the problem.
thanks a lot.
Answers
The PC Device Uploader aspect is found in the Library Structure ...
Library Structure -> PCDeviceLib -> PCDeviceLib <version> ... PCDeviceLibUploader
Opening the aspect can take some time if you have a large project. Run the uploader on all your applications. Make any required corrections as described in the uploader error log and re-run the uploader untill it completes without errors.
what version of minerals libray are you using? Since v5.1/5a you must used "Minerals Library Uploader" aspect from Functional Structure (based on .NET interface), for v5.1/5 or lower you must used Name Uploader, PCC Uploader, Group Uploader aspects from Control Structure (based on Visual Basic interface)
Regards,
Cesar.
Add new comment