Exposed as out terminal not working in Expression Variable
I am trying to access expression variable of a generic element by selecting exposed as out terminal check box while creating the expression variable. It is not working when I call the generic element in the graphic display. Can anyone tell me the procedure to use it? Are there any settings to be done in the system or PG2 editor for the exposed as out terminal to function? I am using System 800xA 5.1 FP4 RevD.
Answers
Hi,
What you have done is Correct. no other settings are required for this option.
See the attchment, i have created one generic element in graphic structure and i created one "Test" Expression variable. i made it as Exposed to Out terminals.
i called the Generic element in graphic display after that you see the Out terminal in screen shot attached.
Best Regards.
I think this is a known issue with FP4 Rev D, you'll need to upgrade to Rev E then it should work.
Add new comment