Controlextendedlib with timeaverageCC control module in CBM
Hi all!
- I need use timeaverageCC control module in CBM. But my system version is 5.1.0, so controlextendedlib do not have that control module. I read it in document, it show that module only have from version 5.1.1.
- If anyone has timeaverageCC control module, Can you send me picture of code, parameter, variable of that control module or import/export for controlextendedlib with that control module?
Thanks so much!
Answers
Only the library owners shall have access to the code of the control module as it is protected library and this may not be shared to others. So if you know the functionality required for your project, you can consider to create your own module based on requirements. I don't see anyother option if you don't want to upgrade the system version.
Add new comment