Licensing options in 800xA
What are the MFG_CLIENT and AC800M_QUANTA licenses and what is the basis of their counts?
Answers
AC800M_QUANTA is related to number of AC800M controllers you can have. PM891 is 100 Quanta points and PM866 is 67 Quanta points.
No idea about MFG_CLIENT. Something related to Batch ??
Googling on AC800M_QUANTA returns hits, one of the first a thread on AKS
http://www402.abbext.com/ac800m-licen...
I believe MFG_CLIENT is some add-on feature to ProduceIT Batch.
After 5.1 licensing is based on ccp so for each controller based on type ac800m_quanta is decided instead of clp in older versions
Add new comment