800xA 5.1FP4 HART Deviceintegration for VEGASON62
Hi,
has anyone successful used the HART Device Integration for Vegason62 Leveltransmitter?
According to ABBs HART Device Datasheet the DTM fo Vegason61 is to be used for Vegsaon Series 61, 62, 63 etc.
We can use the Vegason61 DTM for Vegsan61 transmitters but not for Vegason62 transmitters (via the DTM we can connect to the Device but don't get live Value's)
Answers
please contact dic@in.abb.com with all the details. (including the Device Model, Device ID, Sentinel ID (if applicable), project details)
Add new comment