PPelement Function Block Parameter and Interection Window
Hi,
We are using PPelement v4.0-4 (PID01 block - 800xA).
The last input parameter for this block is the "Param" parameter.
If we expand this parameter, we find Param.HSI_OUT_HL value.
We can write into this value, but the block uses the interaction window value instead.
So what we want to do is change the HSI_OUT_HL by logic but it seems that only by interaction window the change occurs.
How do we do this?
Thank you.
Answers
We have an answer that the PARAM it is just for the first value (cold restart).
So we have to use the inputs that we are used to :
Eolim and Eohl.
Add new comment