800XA import/Export
Hi,
Please, help me?
See Attached file, about error import/export 800XA.
Thank a lot.
Voted best answer
Hello,
Provide the system version & is it problem in all machines have u tried taking backup in Aspect server.
It looks like .Net related issue needs to install & register the dot net framework & allow the server side includes,active server pages,asp.net v2.0 kindly go though the installation manual page 47 onwords.
Answers
Hi,
Some information on above mentioned error i got from one of my IT colleague:-
This error message can be received if the Microsoft .NET Framework component is not installed on your computer, outdated or if it is damaged.
How to resolve:-
Microsoft .NET Framework component should be installed or repaired.
To install or repair Microsoft .NET Framework please do the following:
- Close all open applications.
- Click the Windows Start button and choose Control Panel.
- Double-click Program and Features > Uninstall a program.
- Search the list of currently installed programs for Microsoft .NET Framework
If the program isn't listed, install it:
Download it from the Microsoft website.
If the program appears in the list, repair it:
- Select Microsoft .NET Framework, and then click Change/Remove.
- Select Repair, and then click Next.
- When prompted, restart your computer.
NOTE: If the error persists after installing or repairing, there may be other damaged components to the Microsoft .NET Framework. Uninstalling and then reinstalling Microsoft .NET Framework using the steps in Repairing or reinstalling Microsoft .NET Framework may resolve the issue.
Add new comment