Problem in Importing application from PP245 to PP882
While importing the PP245 application built in Panelbuilder ver 5.1/0 to PP882 in Panelbuilder ver 6.0, following two problems are observed,
1. When the terminal type was selected as PP245 in the application, the importing was stopped in between while importing with errors. And in the same application, when the terminal type is changed from PP245 to PP845, the importing was success.
So, I assume that importing directly from "Process panel (PP1XX,2XX,3XX series)" type to "Panel 800 (PP8XX series)" type is not possible. Is it right ? (please find attached screenshot for error details.)
And, is there any procedure to follow when we upgrade the system from Process panel to Pane 800 series ?
2. After imported the application from version 5.0 to 6.0, all the symbols, texts and object orientation are changed from the original application. Is there any method to restore the disturbed application to original ?
Voted best answer
Hi,
1. Correct, you need to go to version 5 first using Panel Builder 5 and then to version 6 using Panel Builder 6.
2. Please check with support line as well. Normal option is to use the format painter.
Source:
Answers
Hi,
2. using multiple select and changing paramters for all objects works too.
Add new comment