AC31, AC500 Rubric number
Hi guys,
I have a question about Rubric number. What does it mean or what is the difference? Our supplier has got AC31 CPU 07KT94 with number GJR5252100R0161 and we can provide him new CPU with number GJR5252100R0261. Can we replace it with this CPU?
AC500 CPUs have got this Rubric number as well.
Thanks
Voted best answer
Hi,
The CPU with Sno.GJR5252100R0161 and Sno. GJR5252100R0261 differ based on input power and interfaces
If you find the same difference in AC500 PLC's, then they use different versions of Codesys to program them. xxx161 uses lower version (V1.2.1) and xxx261 uses higher version (V2.0 and above).
Thanks & Regards,
Gautham
Answers
Hi
AC31 is a OLD type of ABB PLC, AC500 is a NEW type of ABB PLC.
The two products are not interchangeable between them
Hope this help you
Add new comment