Looking for Aspect Verb references in 800xA
Hello all,
I am looking for something that shows the references of a Aspect Verb, like the Acknowledge Verb of an Alarm List. Is there something where I can see where the Acknowledge Verb of an object is written in the system?
Answers
AFAIK there are two kinds;
1) Embedded verbs
2) Scripted verbs
The verbs from the first category are compiled into the product and can not be dissected; eg the acknowledge verbs.
Verbs from the second category can be viewed/edited. Eg the process operation verbs in 800xA for Advant Master, "On", "Off", ...
/S
Add new comment