Tabbed workplace multiscreen
Hi AKS
I have a tabbed workplace setup with 4 screens aside (not 2x2). The three buttons defined for the tabbed workplace area however appear as if I have a 2x2 setup of screens instead of 1x4.
Does the appearance depends on some setting?
Kind regards
Rune
Answers
Hi Rune
Some time ago I was also „fighting“ with this buttons. As much as I know you can’t configure the Buttons. Button up to 3 screens appears in a row (1x3) and for 4 screens as (2x2).
Finally I am not using this buttons because it is not intuitive for the operator to use one button for different screens. And we are also using 4 Screens in a row.
Now I have the same navigation on each screen, and on each screen you have only the 1-Screen-Button which is navigation only the screen where it’s located on. Also this was not very easy to set up, but you think this would be your solution you try and if you have question you can ask again.
Add new comment