Controlware II PMAP unable to see VFD raw data
I have a PBUS configuration issue. I am able to control my drive through CTK monitoring but cannot manipulate the drive via Controlware II after installing the .PBA. I am trying to map the data to the PMAP arrays. My PBUS and PSLVs are operating and mapped properly. I have two CI840As installed and the RIO is working great. My issue begins when I am trying to integrate a general profibus drive at FIX 1. My PMAP looks to be configured properly, but I cannot see the raw data being published from my drives configured PPO which matches the GSD file loaded in the CTK and Conductor. The PMAP.MOD is pointing to the proper slave as well.
I am running
System - Windows XP, version 2002, SP 3
CTK version - release 6.0
Controlware II version - release 6.0, I believe
Conductor NT - ECC MUX updates 1.0.7
DCU2000G - v7.5.1
DCUsup - v7.6.37 (SR6.0_SP3)
Conductor NT - v6.0.12.0
Answers
Hi
I had a simular problem and I used a totaly new PMAP module and after that everythings worked correctly.
Please just try it, connect your new S800 I/O module to another free PMAP module.
Please let me know when it workes.
Kind regards
Jean-Pierre
Add new comment