800XA Information Manager Data Retrieving
We have 800xA system Version 4.1.Information Management Serevrs .These Servers Archive the Data in iso format and We make the DVDs of that to store data.
Now we want to restor the Historical Data saved in Dvds.What is the process to retriving the data through DVDs.
Moreover ,can we extract the data using ABB data direct Historical Values.
Answers
Should be mentioned in the IM Configuration Manual...
1) Mount media
2) Browse and publish
3) Use regular trends, etc to scope back to the archive time
Published archives should be visible on affected Log Configuration aspects as "Zip" icons for testing purposes (eg Read and export to CSV on the LC's status tab).
DataDirect should be able to read published logs to Excel.
4) Unpublish archives to free up space in Oracle.
Add new comment