CBA 1.4/2 licens problem
Hi
We are running windows 10 Enterprise 2016 LTSB and 800xA 6.0.3-3 on clients. Now we have installed CBA 1.4/2 but I have issues with the license.
When running for example FCB or ONB there will be an invalid licenses window. When I check the log file in the license server it says error 8004ab09.
Is it possible to run this combination ?
Answers
The software can be installed without the license key from Control Builder A version 1.4 onwards.
A license key is required only if either the Function Chart Builder or the On-line Builder is used.
A license must be present in the License Server for each user of these builders.
The following licenses are available: • Control Builder A 1.4 FCB for AC 400 License, one user • Control Builder A 1.4 ONB for AC 400 License, one user
A license key is required only if either the Function Chart Builder or the On-line Builder is used.
A license must be present in the License Server for each user of these builders.
The following licenses are available: • Control Builder A 1.4 FCB for AC 400 License, one user • Control Builder A 1.4 ONB for AC 400 License, one user
The license key is installed in the license server as you can see.
The license key is installed in the license server as you can see.
Add new comment