Connecting PC to acs 355
I want to connect acs355 to PC .I have just usb port.which adapter and driver I need?.when I open drive window light and going to comm setting ,user defined I have one choice which is Com0.how I adjust the communication in my pc?
Answers
Hi
To connect a PC with an ABB ACS355 drive, you need a USB-RS232 converter, a copy of the SW Drive Window Lite and an RJ45-RS232 cable.
During the connection, in the communication options you will have to assign to the communication port the COM value that your PC identifies in the USB-232 converter.
You can check the COM port number in your PC system.
BR
Flavio
To connect a PC with an ABB ACS355 drive, you need a USB-RS232 converter, a copy of the SW Drive Window Lite and an RJ45-RS232 cable.
During the connection, in the communication options you will have to assign to the communication port the COM value that your PC identifies in the USB-232 converter.
You can check the COM port number in your PC system.
BR
Flavio
Add new comment