Automation Builder 2.4: Codesys simulator is not connecting with HMI simulator
Hello,
I am new with ABB...Can't figure why simulator PLC is not connecting CP600 simulator.
What I have done
1- Add symbol configuration
2-build and generate the XML
3-selected Codesys v3 Ethernet protocol.
4-Import tags from the XML .
5-Run the simulator..
Result...is nothing...Tried loop back ip 127.0.0.1..same...
Any advice what should I do ? Or it is not connecting with the simulator!!!!
Answers
Hi,
AFAIK you can simulate both separately. But I don't think you can communicate between two simulations
AFAIK you can simulate both separately. But I don't think you can communicate between two simulations
someone told me ...Simply they are not connecting ... You have to get real PLC... Is it really the case...I am disappointed actually.
Add new comment