Alarm and Event Configuration/800xA 6.1
Hai Everyone,
How to configure alarm and event list that to be displayed in the Application bar in workplace structure. And Is it possible to bring all these alarms and events in
in graphis displays
How to configure alarm and event list that to be displayed in the Application bar in workplace structure. And Is it possible to bring all these alarms and events in
in graphis displays
Voted best answer
Hi. In simple terms, yes.
For the Application bar you need to create an Alarm List and configure to show the values you need (eg Alarm state, priority etc) and filtering as needed. Normally no title bars are used. The Application bar is associated with your Workplace. Find this aspect and modify to show the Alarm list on your Workplace as needed (ie size, order (left to right) etc).
Using the same Alarm List (or any other) you can embed this in any display as an Aspect View within the PG2 graphic system. Note that this does have a performance impact for call-up.
For the Application bar you need to create an Alarm List and configure to show the values you need (eg Alarm state, priority etc) and filtering as needed. Normally no title bars are used. The Application bar is associated with your Workplace. Find this aspect and modify to show the Alarm list on your Workplace as needed (ie size, order (left to right) etc).
Using the same Alarm List (or any other) you can embed this in any display as an Aspect View within the PG2 graphic system. Note that this does have a performance impact for call-up.
Add new comment