Profibus IO cluster with CI801 and SattLine Master CIPB-DP, Firmware,SYCON HMS.
Hello Everyone,
I am using IOs on profibus CIPB-DP profibus Master in SattLine with CI801 DPV1 Slave and setup looks like
CIPB-DP>CI801>AI810:AI810:AI810:AO810V2:DI810:DI810:DO810.
GSD version for CI801 is 1.6
Configurator software is SYCON HMS.
Problem Description:
AO810V2 wont communicate and error I get is that card is not present at position. Card shows constant warning light and I have checked power,lock button, pins and position.
In addition to that CI801 will stop communicating if I will make changes in GSD configuration (module type etc) than I downloaded initially.
Can anyone can suggest me what is factory firmware/software version of CI801 and should it be upgraded in order to work with IO modules mentioned above?
Any compatibility matrix on CI801, IO modules and SattLine Profibus Master card?
Thank You and Regards,
Answers
This question has not yet been answered.
Add new comment