NPT fault
Hi,
When setting up a new 800xA node 6.1.0.1 i get following error (see attached picture)
Anyone having an idea on what it can be?
I the node is connected to domain and the service and installer account has been set up in the domain.
These users are also members in the lokal node administration group.
Thanks
When setting up a new 800xA node 6.1.0.1 i get following error (see attached picture)
Anyone having an idea on what it can be?
I the node is connected to domain and the service and installer account has been set up in the domain.
These users are also members in the lokal node administration group.
Thanks
by Stefan Stromqvist
Members as *direct immediate* members of a group, or indirect by having a security role giving out the group membership?
The code behind these checks in user management is old and may not work if permission is inherited via one or more indirect steps, e.g. via a security role.
by kuhs91 Rank: 380 on 3/30/2021 6:19:33 AM | Like (0) | Report
Problem solved, wrong settings for the GPO not giving the service account the right access
by Stefan Stromqvist
Be warned... this (security handed out by GPOs) have stopped working for some customers for no good reason...
... solution: make accounts direct members of required security groups as the pictures in the users guides show.
Add new comment