RNRP Issus (not visible in rnrp status tool)
I have installed xA6.1 and I am experiencing issues with add node connections.
Aspect Server does not appear in the rnrp of the client system and the same problems occur with the Aspect Server (the client system rnrp of the Aspect Server does not appear). But both system IP are pinging across and another node is showing .
only few system having problem and rest of system is ok.
Aspect Server does not appear in the rnrp of the client system and the same problems occur with the Aspect Server (the client system rnrp of the Aspect Server does not appear). But both system IP are pinging across and another node is showing .
only few system having problem and rest of system is ok.
Answers
Sounds like you have left IGMP snooping enabled in some switch.
IGMP must be disabled for RNRP to work. This is mentioned in the Network Configuration User's Guide.3BSE034463-610
IGMP must be disabled for RNRP to work. This is mentioned in the Network Configuration User's Guide.3BSE034463-610
Add new comment