Firmware upgrade/800xA 6.1
Hi everyone,
How to check the firmware and ip address using tk212 tool cable in pm863(redundant controller)
How to check the firmware and ip address using tk212 tool cable in pm863(redundant controller)
Voted best answer
Hello
You can find a tool "IP Config" in tools of your xA system.
To Check IP address:-
To check firmware:-
There are 2 ways.
The other way is Serial Firmware upgrade
Whenever you reset the controller, the firmware information will be displayed in the popup.
If you want to downgrade the firmware it is recommended to do it in Serial Firmware upgrade tool.
If you want to upgrade the firmware it is always recommend to do it in Remote system only.
You can find a tool "IP Config" in tools of your xA system.
To Check IP address:-
- Terminate both cex slot and rcu slot using terminator
- Press on init button of controller for 2-3 seconds, release the button
- IP Config shows System reset detected and waits for scanning for the IP inside controller.
- You will find both IP as well as subnet mask in the window.
- Make all the relevant changes i.e for backup address, match speed settings and store the IP settings.
- Popup new IP will store appears click OK and exit.
To check firmware:-
There are 2 ways.
- When all communication are established you can directly login to your program
- Right click controller >> Remote system >> Show Firmware information.
- If it promted for update kindly update via remote system only.
The other way is Serial Firmware upgrade
Whenever you reset the controller, the firmware information will be displayed in the popup.
If you want to downgrade the firmware it is recommended to do it in Serial Firmware upgrade tool.
If you want to upgrade the firmware it is always recommend to do it in Remote system only.
Add new comment