Clone a deployed Operator client virtual machine in 800xA SV6.1
Is it possible to clone a deployed Operator client virtual machines in SV6.1? This worked well in SV5.1, but I'm not sure how this will work with the new Node deploy function in the System Configuration Console. The cloning procedure is a as follows:
- Clone the virtual machine;
- Start the clone. Run sysprep (restore all settings to their default settings, but keep the installed software);
- Restart the clone as a new machine. Configure network adapters. Set the machine name, include the machine into the domain.
Voted best answer
It is recommended to create a clone before you deploy any new node into a system; that clone can later be used as a golden image when spawning new nodes or as foundation when having to call "Replace Node" in case something go broken.
Murphy's Law 1st and 2nd law of computers: backup often, backup early.
Murphy's Law 1st and 2nd law of computers: backup often, backup early.
Answers
The answers is No, not supported.
Biggest issue is the 800xA InstallerAgent, and possibly other 800xA related configurations.
So, short answer No.
Biggest issue is the 800xA InstallerAgent, and possibly other 800xA related configurations.
So, short answer No.
Add new comment