S+ 2.1.2 Historian Index Not Generating
Historian archive index not generating. Verified the PWTagSync also not change to "0" after restart the PC. Verified all Historian services are running. Total Historical Tag configured were 2100 tags. Anyone have facing the same issue before? Appreciate your support.
Answers
Hi,
Please remove the time stamp below that entry. If still not updating restart the pwtagsync service.
Also, ensure that the tag database is also cleaned up with the existing Historic Archive Index Default and Historic Archive Identifier are empty.
Change the History long term archive flag with a change from Y to N or N to Y to detect the changes.
Refer to user manual for more information.
Regards,
Farooq
Please remove the time stamp below that entry. If still not updating restart the pwtagsync service.
Also, ensure that the tag database is also cleaned up with the existing Historic Archive Index Default and Historic Archive Identifier are empty.
Change the History long term archive flag with a change from Y to N or N to Y to detect the changes.
Refer to user manual for more information.
Regards,
Farooq
Add new comment