Does anyone know the Configuration of Kepware kepserverex version 6 with Moxa Mgate Mb3660
Does anyone know the Configuration of Kepware kepserverex version 6 with Moxa Mgate Mb3660?
We have 800xA version 6 system which is having Kepware kepserverex version 6 and this Connectivity server is connected with with a Moxa Mgate Mb3660 which reads modbus serial devices. and also there are some direct modbus TCP devices connected to server via switch.
in 800xA we have added the generic opc to read the OPC data from Kepware.
We have configured the Mgate with modbus settings and verofued through the modscan software.
Now we need to configuration in kepware to read these modbus data.
We have 800xA version 6 system which is having Kepware kepserverex version 6 and this Connectivity server is connected with with a Moxa Mgate Mb3660 which reads modbus serial devices. and also there are some direct modbus TCP devices connected to server via switch.
in 800xA we have added the generic opc to read the OPC data from Kepware.
We have configured the Mgate with modbus settings and verofued through the modscan software.
Now we need to configuration in kepware to read these modbus data.
Answers
Hi!
I belevie you have to use the MGate Manager sw to configure and address the Mgate on the Modbus TCP network.
Then, if you have installed the correct Kepware Suite software (i.e. Modbus Suite), you should be able to add a new "Connectivity Channel" using KepserverEX Configuration sw. You have to provide interface configuration, nodes etc etc.
Regards
I belevie you have to use the MGate Manager sw to configure and address the Mgate on the Modbus TCP network.
Then, if you have installed the correct Kepware Suite software (i.e. Modbus Suite), you should be able to add a new "Connectivity Channel" using KepserverEX Configuration sw. You have to provide interface configuration, nodes etc etc.
Regards
Add new comment