irregularities between IEC61850 Utility and 800xa (bad not connected)
Like the pictures in the file. I am missing the logical nodes in IEC61850 Utility, but not in 800xa. I AM aslo using a 3 rd party OPC Scout and reading values from this logial node.
VO1, Vo2, Vo3.
I do something in a test system everything is Ok, but in a live plant which is redundant OPC I am missing the logical node in the IEC61850 Utility.
by ParthibanT Rank: 42 on 3/10/2021 7:55:01 AM | Like (0) | Report
File/Pictures are not attached here
Add new comment