Consistency check on User structure Error Message User information is not updated from Windows user for user
When i want to check the consistency on the User structure i get an error message.
User information is not updated from Windows user for user: XXXX
What could be the problem ?
Its not on all the users. But in the AD the users are configured the same way.
800xA Sv 6.1
User information is not updated from Windows user for user: XXXX
What could be the problem ?
Its not on all the users. But in the AD the users are configured the same way.
800xA Sv 6.1
Voted best answer
IIRC, the Consistency Check code of the user information aspect has a flaw that will raise a false positive if there is a difference in upper/lower case between System 800xA and the Microsoft Windows domain information; "John Doe" vs "JOHN DOE" will trigger an error.
Answers
Just synchronise the user in User Structure, it usually resolves this issue.
Add new comment