Faceplate Resolution Appearance in 1920x1080
I'm running a VM with resolution of 1920x1080, I'm working in Engineering workplace and need to fix the appearance of the faceplate to match my screen resolution (attached Image), i have tried changing the VM resolution, and added 'View Class Mapping' with Wide Screen configurations, but did not work.
Thanks for the support.

Thanks for the support.

Answers
If this is a VM in a workstation or laptop, VMware Workstation have a rescaling feature that may mess up things, also,
in Windows 10 there is settings for scaling that can mess things up.
in Windows 10 there is settings for scaling that can mess things up.
by ParthibanT Rank: 42 on 3/4/2021 5:25:02 AM | Like (0) | Report
Pls check Display Settings like Scale and Layout etc.,
by ParthibanT Rank: 42 on 3/4/2021 9:02:54 AM | Like (0) | Report
Use size display aspect and find out the resolution from xA point of view.
by Ghaith Al Rousan Rank: 1402 on 3/6/2021 12:42:37 AM | Like (0) | Report
I have changed the display setting scale from VM settings and windows settings. when i open the Engineering workplace initially, the scale if ok and there is no issue, however, when i navigate and open any faceplate, the resolution of the whole engineering workplace is increase and the scroll bars appear. i,e. if i initially work on other structures such as service structure, the workplace scaling if fine.
where can I use the Size Display aspect? i have checked the Faceplate configuration in library structure, but could not add size display aspect.
Add new comment