Problems reading from IED with v6.1 IEC 61850
Hi
I have somw problem swith readingthe data from a relay with version V6.1?
Some data in a RCB are ok, and some are not.
I have somw problem swith readingthe data from a relay with version V6.1?
Some data in a RCB are ok, and some are not.
Answers
Hi
I have imported a SCD file from Schneider Easrgy P3F30 relay. I have used IED Scout and the data seems ok, but the data is inconsistant when transfer over to 800xa. See screenshot for IEC61850 utility.
There is some information on timestamp, where I have value N=1 and N=0 on some DOsignals.
I am not sure where the fault is.
I have imported a SCD file from Schneider Easrgy P3F30 relay. I have used IED Scout and the data seems ok, but the data is inconsistant when transfer over to 800xa. See screenshot for IEC61850 utility.
There is some information on timestamp, where I have value N=1 and N=0 on some DOsignals.
I am not sure where the fault is.
by ParthibanT Rank: 42 on 3/1/2021 1:04:07 AM | Like (0) | Report
Problem description is Very short or not clear, add screenshots if available for better understanding.
Add new comment