Can we Disable SMBv1 service in 800XA Nodes
Windows 2016 server + 800xa 6.1 + 800XA History
Can we Disable SMBv1 service in 800XA Nodes ?
Answers
Hello,
here is an extract from the 800xA Security Deployment Guide for 800xA 6.1:
9 System Hardening – Remove SMBv1
SMBv1 protocol is very old protocol and its no longer supported by Microsoft. SMBv1 has many known vulnerabilities which were exploited for example Wannacry or Wannacrypt. Refer to Cyber Security Notification WannaCry (9AKK106930A9737). Its strongly recommended to remove SMBv1 protocol using the following procedures: Note: A node reboot is needed after the below procedures. Plan the activity accordingly on a running system.
br
Reinhard
here is an extract from the 800xA Security Deployment Guide for 800xA 6.1:
9 System Hardening – Remove SMBv1
SMBv1 protocol is very old protocol and its no longer supported by Microsoft. SMBv1 has many known vulnerabilities which were exploited for example Wannacry or Wannacrypt. Refer to Cyber Security Notification WannaCry (9AKK106930A9737). Its strongly recommended to remove SMBv1 protocol using the following procedures: Note: A node reboot is needed after the below procedures. Plan the activity accordingly on a running system.
br
Reinhard
Add new comment