AfwWorkplaceApplication.exe fails to start up
We get the following errors (see attachment) when starting the AfwWorkplaceApplication with the default workplace on an engineering station type computer.
This seems to have happened after installing Windows updates i.e. it worked fine before installing the updates.
This seems to have happened after installing Windows updates i.e. it worked fine before installing the updates.
Answers
Have you installed MS hotfixes which are certified by ABB or the complete set of MS Hotfixes?
Only certified Hotfixes are allowed to be installed!
br
Only certified Hotfixes are allowed to be installed!
br
Hi!
Can you start any workplace or is this problem only with the default workplace? Only on this computer?
How is the workplace started, via Windows task scheduler or?
If you start that workplace as that user on that computer manually, is this what happens?
If you go into plant explorer, Workplace Structure, find that workplace, right click on that object, chose launch, does it start as it should?
With Regards
/N
Add new comment