RTU560-CMU05 unreachable except by default IP address
Problem of access to the web server using the configured ip address (even the ping doesn't work) on both Ethernet interfaces (E1 and E2).but when using the default ip address (with the jumper on Pins1-2) ; the ping is possible on the 192.168.0.1 and the web server works.
Answers
This question has not yet been answered.
Add new comment